Wiki pages that were migrated are redirecting to the new location. Pages not migrated are only accessible to users on the TI network. Users off the network can not access the Wiki and will receive a 404 error. DO NOT share Wiki URLs with customers. They can not access the Wiki site.
TCI6616/C6670/TCI6608/C6678/TCI6618 Device simulator User Guide
Contents
[hide]- 1 Purpose
- 2 Simulator Configurations
- 3 Simulator installation
- 4 Simulator Selection & Configuration
- 5 Simulation Features
- 6 Device simulator -- IP model details
- 7 Cycle Accuracy of Simulator
- 8 Virtualized IO
- 9 IP Model Details
- 9.1 C66x ISA
- 9.2 C66x CorePac
- 9.3 RSA
- 9.4 Multi-core Shared Memory controller (MSMC)
- 9.5 EMIFv4 - DDR3
- 9.6 Semaphore
- 9.7 PSC
- 9.8 Device Status Control Register
- 9.9 EDMAv3
- 9.10 RAC2
- 9.11 TAC
- 9.12 VCP2
- 9.13 TCP3D
- 9.14 TCP3E
- 9.15 FFTC
- 9.16 Multicore Navigator
- 9.17 PCIe
- 9.18 UART
- 9.19 SRIO
- 9.20 Network Co-processor
- 9.21 BCP
- 9.22 GPIO
- 9.23 Timer 64
- 9.24 Interrupt Controller
- 10 Limitations
- 11 Related Documents
- 12 Reporting Issues
- 13 Update Releases
Purpose[edit]
The purpose of this document is to walk the user through the various aspects of TCI6616/C6670/TCI6608/C6678/TCI6618/C6657 device simulators, available with Code Composer Studio. This includes:
- Overview
- Simulator Configurations
- Installing the Simulator
- Details of the models that constitute the simulator
Simulator Configurations[edit]
Based on the modeling-abstraction level (details modeled in the simulation), the TCI6616/C6670/TCI6608/C6678/TCI6618/C6657 Device simulators are classified as
- Functional simulator configuration
- Cycle Approximate (CX) simulator configuration
Device simulator categorized based on different abstraction level Configuration Scope Key Benefits
Functional Simulator
- Functional and Bit-accurate
- Model the functionality of CPU, cache, DMA, co-proc and peripherals
- Model the device memory map.
- The application binary run on simulator can be run on Hardware and vice-versa
- Faster Platform (than RTL and pre-si hardware emulators)
- Whole application system creation; OS, device driver support
Cycle Approximate (CX) simulator
- Cycle Accurate and Bit Accurate
- Application performance measurement and tuning
The following is the list of device simulator configuration supported
TCI6616
- TCI6616 Functional Device simulator configuration, Little Endian
- TCI6616 Functional Device simulator configuration, Big Endian
- TCI6616 Cycle Approximate Device simulator configuration, Little Endian
- TCI6616 Cycle Approximate Device simulator configuration, Big Endian
C6670
- C6670 Functional Device simulator configuration, Little Endian
- C6670 Functional Device simulator configuration, Big Endian
- C6670 Cycle Approximate Device simulator configuration, Little Endian
- C6670 Cycle Approximate Device simulator configuration, Big Endian
TCI6608
- TCI6608 Functional Device simulator configuration, Little Endian
- TCI6608 Functional Device simulator configuration, Big Endian
- TCI6608 Cycle Approximate Device simulator configuration, Little Endian
- TCI6608 Cycle Approximate Device simulator configuration, Big Endian
C6678
- C6678 Functional Device simulator configuration, Little Endian
- C6678 Functional Device simulator configuration, Big Endian
- C6678 Cycle Approximate Device simulator configuration, Little Endian
- C6678 Cycle Approximate Device simulator configuration, Big Endian
TCI6618
- TCI6618 Functional Device simulator configuration, Little Endian
- TCI6618 Functional Device simulator configuration, Big Endian
- TCI6618 Cycle Approximate Device simulator configuration, Little Endian
- TCI6618 Cycle Approximate Device simulator configuration, Big Endian
C6657
- C6657 Functional Device simulator configuration, Little Endian
- C6657 Functional Device simulator configuration, Big Endian
Simulator installation[edit]
Prerequisite[edit]
- Win XP
- Code Composer™ Studio
- Code Composer™ Studio v5, or a later version preferred.
- Code Composer™ Studio v5, or a later version preferred.
- Windows Packet Capture (WinPcap) v 4.0.2 or above -- http://www.winpcap.org/install/default.htm
- Note: Needed only in case of using Virtualized IO feature to stream Layer 2 Ethernet packet to/from your m/c ethernet socket
Preferred machine configuration[edit]
- 2.4 GHz processor or above
- 2GB Memory or above
Release Package and installation
[edit]
- The simulator release is available as self-extracting installer.
Note: While installing this simulator release on
- CCS v5 installation, select the Code Composer Studio™ installation path(<CCSv5.x_install_path>\ccsv5\ccs_base_5.x.x.xxxxx\) when the installer prompts for simulation installation path.
Simulator Selection & Configuration
[edit]
Functional simulator Selection & Configuration
[edit]
- Bring up CCS & click on Target->New Target Configuration
- Specify the target configuration file name & use shared location or store it in the project folder.
- Target selection will appear. Select connection type as Texas Instruments Simulator & type the device you are interested in the device filter window (e.g. TCI6606)
- Select appropriate simulator configuration from the filtered list and press the Save buttont to save the configuration.
Cycle Approximate simulator Selection & Configuration
[edit]
- The steps for configuring the Cycle Approximate simulator is same as the Functional simulator configuration, except before saving the configuration you are expected to select the appropriate DDR memory configuration
- Click on the 'Target configuration' to setup the DDR configuarion
- Click on any one of the DSP name under the All Connection window.(step 1, as highlighted in the diagram below)
- This will display a list of configuration which also includes the DDR configuration. Select the desired DDR configuration (step 2, as highlighted in the diagram below) and click on Save button (step 3 as highlighted in the diagram below) to save this configuration
Simulation Features
[edit]
- Supported on CCS [ Refer page http://processors.wiki.ti.com/index.php/CCSv5_Getting_Started_Guide on "CCSv5 Getting Started Guide"]
- Basic multi-core CCS debug and execution capabilities [ Refer page http://processors.wiki.ti.com/index.php/Multi-core_simulator_configuration_semantics on "Multi-Core Semantics on Simulator"]
- CIO, Breakpoints, register, memory windows
- Synchronous and Asynchronous execution of cores
- Global and local breakpoints
- Advanced debug capabilities
- Code Coverage,, Cache Tag RAM view, Multi-level memory hierarchy visibility,
- Analysis capabilities
- Function profiling with interrupt awareness
- Code coverage, Cache & device events
- EMAC and SRIO IO virtualization
- UART connectivity to TCP/IP terminal
Device simulator -- IP model details[edit]
| IP Block |
TCI6616 |
C6670 |
TCI6608 |
C6678 |
TCI6618 | C6657 |
|---|---|---|---|---|---|---|
| CPU | 4 C66x | 4 C66x | 8 C66x | 8 C66x | 4 C66x | 2 C66x |
| CorePac | Yes | Yes | Yes | Yes | Yes | Yes |
| RSA | Yes | Yes | NA | NA | Yes | NA |
| MSMC | Yes | Yes | Yes | Yes | Yes | Yes |
| DDR3 EMIF | Yes | Yes | Yes | Yes | Yes | Yes |
| Debug & Trace | No | No | No | No | No | No |
| Boot ROM | No | No | No | No | No | No |
| Semaphore | Yes | Yes | Yes | Yes | Yes | Yes |
| Power Management | ||||||
| PSC Registers | No | No | No | No | No | Yes |
| Device State control Register | ||||||
| Inter process communication registers | Yes | Yes | Yes | Yes | Yes | Yes |
| Others | No | No | No | No | No | No |
| PLL | No | No | No | No | No | No |
| EDMA | Yes | Yes | Yes | Yes | Yes | Yes |
| RAC | Yes | Yes | NA | NA | Yes | NA |
| TAC | Yes | Yes | NA | NA | Yes | NA |
| VCP2 | Yes | Yes | NA | NA | Yes | Yes |
| TCP3d | Yes | Yes | NA | NA | Yes | Yes |
| TCP3e | Yes | Yes | NA | NA | Yes | NA |
| FFTC | Yes | Yes | NA | NA | Yes | NA |
| Multi-core Navigator | ||||||
| Queue Manager | Yes | Yes | Yes | Yes | Yes | Yes |
| Packet DMA | Yes | Yes | Yes | Yes | Yes | Yes |
| I2C | No | No | No | No | No | No |
| PCIe | Yes | Yes | Yes | Yes | Yes | Yes |
| UART | No | No | No | No | No | Yes |
| SPI | No | No | No | No | No | No |
| AIF2 | Yes | Yes | Yes | Yes | Yes | No |
| SRIO | Yes | Yes | Yes | Yes | Yes | Yes |
| Network Co-processor | ||||||
| Ethernet Switch | Yes | Yes | Yes | Yes | Yes | Yes |
| Packet Accelerator | Yes | Yes | Yes | Yes | Yes | Yes |
| Security Accelerator | Yes | Yes | Yes | Yes | Yes | Yes |
| Hyperlink | No | No | No | No | No | No |
| BCP | NA | NA | NA | NA | Yes | Yes |
| GPIO | NA | NA | NA | NA | NA | Yes |
| TIMER64 | Yes | Yes | Yes | Yes | Yes | Yes |
| INTC | Yes | Yes | Yes | Yes | Yes | Yes |
The following pictures summarizes the sections that are modeled/not-modeled in TCI6616, TCI6608, TCI6618 and C6657 simulator configurations.
Cycle Accuracy of Simulator
[edit]
The following table summarizes the different category of models, classified based on the degree/details of accuracy models, and the IP models in the Device Cycle Approximate simulator configuration that are modeled for it.
IP Model Category
Accuracy w.r.t RTL
IP Models in TCI6616/C6670/TCI6608/C6678/TCI6618 Devices
Cat3: Programmers-view (PV) model
- No Accuracy.
NA
- SRIO, GPIO,
- INTC,
- VCP2, TAC, RAC,
- Queue Manager
- RSA
- Boot ROM
- Network Co-processor
- IPC, Semaphore,
Cat2: PV with Timing (PVT) models
- Computation-time-accurate models
>75%
- PKTDMA,
- TCP3D, TCP3E,
- FFTC
Cat1: Highly cycle-accurate models
- Arbitration, Priority and pipelines are modeled to match the micro-arch details
>90%
- C66x ISA,
- CorePac Memory System (L1+L2),
- MSMC, DDR-EMIF,
- EDMAv3, Timer
- AIF2 Timer module
Cat0: RTL-to-C converted models
100%
None
Cycle Approximate Simulator bus-topology details.[edit]
Since the IP models in the Device Cycle accurate simulator are modeled at different abstraction level (as summarized in the table above), the simulator bus-topology uses a mix of interconnect as depicted in the following diagram
Cycle Accuracy Validation Process
[edit]The cycle accuracy is measured and calibrated against the RTL/Silicon w.r.t a set of identified benchmarks/test-cases
Cycle Accuracy Results
[edit]The following table summarizes the cycle accuracy acheived on the Cycle Approximate simulator configuration.
Scenarios/Paths
Achieved Cycle Accuracy
CPU w/ 100% L1D and L1P Cache/SRAM
100%
CPU w/ accesses within L2 Cache controller
95%
CPU w/ accesses to MSMC
90%
CPU w/ accesses to DDR
80%
EDMA transfers involving internal, shared and external memories
80%
Virtualized IO[edit]
The TCI6616/C6670/TCI6608/C6678/TCI6618 Device simulator supports Virtualized IO capabilitied for the following IP models.
- SRIO
- Ethernet Switch
SRIO Message Passing Support
[edit]
- SRIO Type 11 messages encapsulated in TCP headers can be passed into and out of the simulator
- SRIO physical layer is not modeled
- Dedicated port routes TCP packets to a socket in the simulator that strips the TCP header and forwards the SRIO message to the SRIO port 0
- User’s application on PC produces and consumes SRIO messages tunneled over TCP
- TCI6616/C6670/TCI6608/C6678/TCI6618 Device Simulator SRIO Model User Guide contains configuration details and packet structure
Simulator Ethernet Connectivity
[edit]
- The EMAC Model in the Device simulator supports Layer 2 (Data Link Layer) messaging over the network.
- Ethernet packet transmission and reception
- It uses the WinPCAP library to interact with the network. The EMAC will capture Ethernet packets based on the MAC address configured in the simulator configuration file.
- Broadcast packets are also forwarded to the simulator.
- Details contained in Device Simulator EMAC Model User Guide.
IP Model Details
[edit]
C66x ISA[edit]
What is Supported? What is not Supported?
- C66x ISA
- Interrupts and Exceptions
Note: It is recommeded to use Cycle approximate simulator configuration for benchmarking purposes because the functional simulator does not support CPU cross-path stalls.
C66x CorePac[edit]
What is Supported? What is not Supported?
- L1/L2 Cache controller
- Interrupt Selector, IDMA
- Extended Memory Controller
- Cache and memory simulator statistics
- Clock Speed: C66x CorePac runs at
1 GHz Clock
- The following bits in the MAR registers, and its associated
functionality is not supported
- WTE bit – selects
between write-back (0)
and write-through (1)
caches in
DMC/PMC/UMC- PCX bit – disables (0)
and enables (1) caching
in MSMC RAM (not
committed)- PFX bit – disables (0) and
enables (1) prefetching in
XMC.
- XMC
- XMC registers
- Address translation
functionality at XMC is
not supported- Memory protection
functionality
RSA[edit]
What is supported? What is not supported?
- RSA functionality
[edit]
What is Supported? What is not Supported?
- MSMC RAM
- MSMC registers
- Address translation functionality
at MSMC*- 36-bit addressing mode*
- CFGLCKSTAT and
CFGLCK register
functionality*Supported on functional simulator configurations only
EMIFv4 - DDR3[edit]
What is supported?[edit]
- The following DDR memories are supported(selectable before the simulation starts)
- DDR3 - 1333
- DDR3 - 1600
The timing parameters used for these memories are listed in the table below.
Description DDR-1600 DDR-1333 SDRAM burst length(in bytes)
8 8 Number of internal banks 8 8 Depth of command FIFO
16 16 Depth of read response fifo
22 22 Depth of write response
7 7 Depth of write data fifo
24 24 Data bus width between EMIF4 and memory(in bits)
64 32 System Interface data bus-width (in bits) 256 256 Page Size(in KB)
2048 2048 Memory clock period (in picoseconds) 1250 1500 EMIF Phy latency 3 3 SDRAM refresh period in number of memory clock cycles 6250 6250 SDRAM size in MB 256 256 Minimum number of mem_clk cycles from activate to precharge - 1
(t_ras)
28 28 Minimum number of mem_clk cycles from activate to activate - 1
(t_rc)
38 38 Minimum number of mem_clk cycles from refresh/load_mode to refresh or activate - 1
(t_rfc)
88 88 Minimum number of mem_clk cycles from precharge to refresh/activate - 1
(t_rp)
10 10 Minimum number of mem_clk cycles from activate to activate to a different bank - 1
(t_rrd)
6 6 Minimum number of mem_clk cycles from the last read command to precharge - 1
(t_rtp)
6 6 Minimum number of mem_clk cycles from last write transfer to precharge - 1
(t_wr)
12 12 Minimum number of mem_clk cycles from last write to read - 1
(t_wr)
6 6 CAS latency (cl)
10 9 Write latency(wl) 8 7 Synchronizer latency 3 3 (t_ccd)
4 4 Minimum number of mem_clk cycles from activate to read/write - 1 10 10 Threshold to do back2back writes before reads 5 5 Threshold to do back2back writes before reads 3 3 What is not supported?[edit]
- EMIFv4 MMR
- 36-bit addressing
Semaphore[edit]
What is supported? What is not supported?
- 32 independent semaphores.
- Direct, Indirect and combined mode for semaphore acquisition.
- Queued requests for used semaphores
- Semaphore access grant interrupt for queued request
- Allows the application to check the status of semaphores.
- Error detection and interrupts
PSC[edit]
What is supported? What is not supported? * PSC Register Only Model * Power/Module enabling bit toggles
Device Status Control Register
[edit]Inter Processor Communication[edit]
What is Supported? What is not Supported?
- IPC registers and associated functionality
- Interrupt output capability to an external host via device pin
(HOUT)
Others
[edit]
What is supported?
What is not supported?
- JTAGID
- DEVSTAT
- KICK0, KICK1
- DSP_BOOT_ADDRx
- MACID
- LRSTNMIPINSTAT_CLR
- RESET_STAT_CLR
- BOOTCOMPLETE
- RESET_STAT
- LRSTNMIPINSTAT
- DEVCFG
- PWRSTATECTL
- TINPSEL
- TOUTPSEL
- RSTMUXx
- MAINPLLCTL0
- DDR3PLLCTL0
- PAPLLCTL0
- PKTDMA_PRI_ALLOC
EDMAv3[edit]
What is Supported? What is not Supported?
- TPCC and TPTC MMR and associated functionality
RAC2[edit]
What is supported? What is not supported?
- RAC2 MMR and associated functionality
TAC [edit]
What is supported? What is not supported?
- TAC MMR and associated functionality
VCP2[edit]
What is supported? What is not Supported?
- VCP2 MMR and associated functionality
TCP3D[edit]
What is supported? What is not supported?
- TCP3d MMR and associated functionality
- Error interrupt
TCP3E[edit]
What is supported? What is not supported?
- TCP3e MMR and associated functionality
- Error interrupt
FFTC[edit]
What is supported? What is not supported?
- Supports IFFT and FFT
- Sizes
- 2a x 3b for 2 = a = 13, 0 = b = 1 – maximum 8192
- 12 × 2a × 3b × 5c for sizes between 12 and 1296
- 16 bits I/ 16 bits Q input and output
- Dynamic and programmable scaling modes
- Support for "FFT shift" (switch left/right halves)
- Output data scaling
- Ping/Pong input, output buffers
- Support for cyclic prefix (addition and removal)
[edit]
What is supported? What is not supported?
- Queue Manager
- Packet DMA
- Timer
- Accumulator PDSP
- Interrupt Distributor
- Linking RAM
- Queue Proxy
- Multi-channel DMA
PCIe[edit]
What is supported? What is not supported? * Register Only Model
UART[edit]
What is supported? What is not supported? * Support to connect TCP/IP terminals like putty/TerraTerm/Hyperterminal
SRIO[edit]
- What is supported?
- What is not supported?
- Logical and Transport layer SRIO
- functionality is supported
- SRIO Port 0
- Message passing SRIO packets (Ftype = 11)
- Type 9 SRIO packets
- SRIO Tx and Rx is emulated thru reads and writes to TCP sockets
- 8-bits and 16-bits device ID
- Refer to TCI6616 Simulator SRIO model user guide for details.
- Physical layer functionality
- SERDES
- SRIO Port 1, 2 and 3
- SRIO packet formats other than Ftype = 11 (Direct IO, Retry logic, Maintenance packets, Doorbell operation, Cache coherence function) and Ftype = 9
- Packet prioritization and reordering
- Multicast device ID
- Transmit and Receive teardown
Network Co-processor[edit]
Packet Accelerator Sub-system[edit]
What is supported? What is not supported?
- Independent Enhanced Packed Data Structure Processor cores (EPDSP)
- 16-bit timers for use by the EPDSPs
- Chunk Data Engines
- 1st pass Lookup Table accelerators
- 2nd pass lookup table accelerator
- Basic Security Accelerator (NULL mode processing) with packet ingress/egress. This Security accelerator does not perform any encryption/decryption on packets, but passes it as-is.
- Complete Cryptography Engine
Switch-Subsystem[edit]
What is supported?
What is not Supported?
- 10/100/1000 Mbps modes (but not at speed)
- Basic Address Lookup Engine
- SERDES configuration
- Rx and Tx Statistics update
- Maximum frame size 9500 bytes
- CRC32 generation and validation
- Supports Layer 2 (Data Link Layer) messaging over the network
- Ethernet packet transmission and reception
- MDIO
- Flow control
- APO (Adaptive performance optimization)
- Packet prioritization
- Packet forwarding
- ALE advanced features (Super, secure and block bits)
BCP[edit]
What is supported? What is not supported?
- Bit co-processor functionality
- Supports LTE, WiMAX, WCDMA (FDD), WCDMA (TDD) -- UL and DL
GPIO[edit]
What is supported? What is not supported?
- GPIO MMR and associated functionality
Timer 64[edit]
What is Supported? What is not Supported?
- Timer64 MMR and associated functionality
Interrupt Controller[edit]
What is supported? What is not Supported?
- CP INTC functionality
- One-to-one mapping of channels with host interrupts for all the INTC instances supported.
Limitations[edit]
Functional Simulator Limitations[edit]
- Refer to "IP Model Details" for the list of IP model limitations
- Refer to the simulator release notes for list of known/pending defects .
Cycle Approximate Simulator Limitations[edit]
- The MMR of the following IP models are not supported in CX simulator
- MSMC
- XMC
- EMIFv4
- Debugger Limitation
- Debugger Reset is not supported
- User should quit the simulation and invoke it again
- Loading Program (coff) from a core, into other core’s internal memory is not
supported. In similar lines,
- The viewing the contents of other core’s internal memory from a given core is not supported
- Mapping the CIO buffer’s into to other core’s internal memory and executing the application from a given core is not supported
- When TCI6616/C6670/TCI6608/C6678/TCI6618 Device cycle-approximate simulator used in a CCS v5.0 environment, you may notice insufficient process memory error, while running large simulation. This is because of a process-memory limit enforced by the operating-system.
- Refer to "IP Model Details" for the list of IP model limitations
- Refer to the simulator release notes for list of known/pending defects .
Related Documents[edit]
- Simulator Release notes
- TCI6616/C6670/TCI6608/C6678 Device Simulator SRIO Model I/O user-guide
- TCI6616/C6670/TCI6608/C6678 Device Simulator EMAC Model I/O user-guide
- UART_Model_user_guide
- Software Manifest Documents
- TCI6616/C6670/TCI6608/C6678DeviceSims SW Manifest 2010
- TCI6616/C6670/TCI6608/C6678DeviceSims SW Manifest 2010 (CCS direct)
Reporting Issues[edit]
Use the link below to file a defect/query on simulator
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81.aspx
Update Releases[edit]
| Version | Date | CCS5 stream | Windows | Linux | Release Notes | Comments/readme |
| 1.0.1.6 | 07/01/2011 | CCS5.0.3 |
Patch over
|
Patch over |
Support for register trace in CPU models. | Readme for Sim CSP installation over CCS5.0.3
|
| 02/07/2012 | CCS5.1.1 | Register trace feature is available in CCS5.1.1 base installation. No patch update required. | Register trace feature is available in CCS5.1.1 base installation. No patch update required. |